This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: BQ76952 电流波动剧增引起故障

Part Number: BQ76952


老师,您好!

根据 BQ76952EVM评估板的原理图,我设计了一款76952的最小系统板,目的是对76952的全温特性精度,

考虑供电电流变化引入噪声对76952 ADC的影响,应用中将CELL16与76952 Vbat供电分离开,并在VSS与CELL0处共地,其余未用引脚均按照手册要求浮空或者接地处理,见下图

现象1:单板调试CELL16-CELL0全浮空,VBat 12V供电输入,初始观测GW开关电源 电流值为1~2mA(开关电源电流显示精度较差),

大约3min左右,电流开始波动4mA,并缓慢波动上升至6~7mA,最终10mA左右,开关电源模块因设置限流禁止输出(12V@20mA),遂关闭电源;

现象2:实验条件如现象1布置,使用MCU对76952通过IIC进行初始化配置,初始REG1与REG2在设定电压3.3V左右,大约2min左右,电压开始波动变化,其中REG1跌降至0.8V电压左右;

在观察Vbat供电,电流约上升到7~8mA,BQ76952 IIC停止工作,且示波器观测测出SCL/SDA电压为0V左右,SCL与SDA被强拉低;

另MCU端SCL与SDA均有上拉电阻4.7K到3.3V,整个故障过程中bq 76952 REG18电压均在1.8V左右,正常

不知问题原因在哪里?希望能得到您的回复,谢谢

另将BQ76952 VBAT供电断开,开关电源显示电流为0mA,说明电路板无其他元件取电,电流消耗在BQ76952芯片处