This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28180: PFC+LLC电源架构,空载上电后切满载正常运行,带载直接上电PFCmos损坏

Part Number: UCC28180


设计一款500W输出PFC+LLC电源,PFC采用UCC28180直驱控制,输入175-265V,输出400V,电感1.1mH,电容330uF,频率105k,LLC启动阈值电压为390V;环路设置按照此芯片计算表格设置。

当我先空载上电,然后再切换至500W输出,切换瞬间PFC输出电压从400V掉至340V,但可正常运行;但是当我带负载直接上电时,电源出现mos及熔断器烧毁。

1.从规格书中得知UCC28180输出电压达到98%软起才结束,LLC启动电压应设置在UCC28180软起结束后吗?

2.切载瞬间PFC电压在LLC开启后下掉60V,增大电容至480uF,下掉仍有50V,是否正常?是否有其他方法减少?

3.如果电压下掉至低于输入整流后的电压,预充二极管导通,会带来什么后果?

4.输出电压采样规格书推荐1MΩ分压,但是我在TI其他文档看到采用10MΩ,是否有影响?