Other Parts Discussed in Thread: TPS23861
该款PSE IC 上说明了 2 线对或 4 线对端口功率分配,目前我们需要采用2线对的方式对PD设备进行供电,但下图种=中2线对功率分配最高只能是30W,而我们这边的设计PD需要的功率为40W,无法满足PD的功率需求,请问2线对端口供电最大功率能提升到40W吗

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
请教一下PSE芯片(TPS23861)对外部非PD设备供电的问题,我们有需求需为非802.3axxx 负载(即没有 PD 的负载)接通电源,负载需要40W左右的功率,我们采用手动模式,关闭端口检测分级功能(利用I2C操作寄存器0X14),更改ICUT (mA)电流为754mA(或者是最大阈值电流920mA), 我们VPWR供电54V,所以
最大功率输出①: 54*0.754=40.7W 或者
最大功率输出②: 54*0.920=49.68W
通过操作寄存器0X19来对端口供电进行打开与关断,请问您我们这样设置,能达到我们所需的高功率(40W)供电需求目吗?