This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如题bq76952可以配置成检测到错误但不会去关闭打开充放电管,bq4050是否有这类功能?
您好,
您的问题我确认下给到您答复。
您是指bq4050是否有通过 GPIO 来关闭保护 FET的方法吗?
你好,我想问的是,例如遇到电池低电压的情况,可不可以只把CUV位置1,而不去关闭mos管。
也就是说触发了这类警报之后,只将警报的标志位置1,不去保护FET
BQ4050和BQ76952的工作方式不同,是由固件控制的。 如果在 Safety Status 中设置 CUV,那么固件将关断 DSG FET。
您可以试下将 CUV 延迟设置为更高的数字(最大255秒),这样 FW 需要更多的时间来关断 DSG FET。 用户可以在未设置安全状态时读取安全警报寄存器。
Thanks