Part Number: BQ2947
请教一下各位专家,这是我设计的3串锂电池保护方案。
我有一个疑问,当电池电压超过11.50V时(每节电池的电压几乎相同),BQ294700的OUT引脚就会输出高电压。
我在规格书中看到,BQ294700的OVP电压是4.35V,所以,3串锂电池的OVP电压应该是13.05V。
我应该如何修改我的设计?谢谢!

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.