This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TPS65381输入电压的疑问?

在使用TPS65381时,当输入电压为5V时,TPS65381无法正常工作,5V、3.3V、1.2V 等均没有输出。

当把输入电压调整至5.6V左右时,上电,TPS65381才能正常启动工作,在正常工作时若将输入 电压调低到5V,芯片依然可以正常工作。

查找datasheet,在4.3中提到“R1.1 Input supply voltage range on VBATP pins for initial power up min 5.8 V” 是否指TPS65381启动时电压必须达到5.8V,否则无法正常启动。

而datasheet中提到的
5.8 V to 36 V (CAN, I/O, MCU Core, and Sensor Supply Regulators Functional)
4.5 V to 5.8 V (3.3-V I/O and MCU Core Voltage Functional)  是指用5.8V输入电压启动完成后,芯片可接受的电压范围。

也就是说TPS65381上电时需要5.8V电压?