在仿真中当LM3150输入10V-34V,输出8.4V时最大电流是7A,但是在电路板上轻松实现8A的电流输出,这是为什么呢?LM3150的最大电流是多少?LM3150的高温保护只是测的是芯片?还是连MOS一起测问题?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,您是用的什么仿真? LM3150只是controller, 其最大电流限制通过ILIM来设置。
建议你用Webench做个设计,对比下看看电路有什么问题。
我想请教一下,lm3150的文档说有过压保护,是电压超过42V就内置电路启动保护将其EN引脚置地从而关断整个电路???假如我想通过另加一个外围电路来做过压和欠压保护,当触发后会使lm3150的en引脚拉低,从而控制lm3150关断起到保护作用,请问有没有相应的ic可以做到相应功能的??谢谢哈