This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1: Power save shutdown及其他shutdown的詳細設置

Part Number: BQ40Z50-R1


您好,

想詢問一下關於shutdown的詳細應用及設置,以下的理解幫忙確認一下對不對,主要是PS shut down的設置條件。

電芯最低放電電壓為2.5V

0%設定為3.4V (term V) (客戶關機電壓在3.3V~3.4V)

CUV設置為3V

Shutdown V 設定為2.9V

PS shutdown V是否設定的區間為0%至CUV之間? ex. 3.2V

而電芯最低不得低於2V,PF shut down則設置在1.8V~1.9V(如發生必須退回原廠解除)

再麻煩協助,謝謝!!