Other Parts Discussed in Thread: LM25118, LM5118, LM5116
使用LM25116芯片输入24V输出4V电源,作为板卡的第一级电源,在经过-2KV浪涌后,4V输出这里有一个明显的跌落;而同板卡上使用LM25118芯片,输入24V输出12V,也是第一级电源,在经过-2KV浪涌后,12V输出这里很平稳,没有跌落现象;然后两个芯片属于同系列芯片,所以跟LM25116芯片的周边参数配置有关?还是跟两个芯片电源输入范围不同有关(LM25116芯片输入最低到6V,LM25118芯片输入最低到3V)?如何能提高LM25116芯片的抗浪涌能力?
两个芯片设计原理图:
-2000V浪涌,用示波器测到输出端波形如下: