This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62816-Q1: 测试的输出纹波与SPEC上的差异。

Part Number: TPS62816-Q1

你好,我们客户在测试的时候发现,下边case 的情况下,输出的纹波与SPEC上给出的不一致,测试的纹波在12mV左右,但是SPEC给出的输出纹波2.6mV,请问输出电容是按照下边的typical application 3*22uF,还是按照EVM的参数??请帮忙解答下,谢谢。

  • Hi

       无论是参考datasheet上电路还是评估板都是可以的,推荐是后者,一般datasheet的电路是来自评估板, 输出是建议3个22uF.

       对于输出纹波无论是几个mV还是十几个mV都是没有问题的,一般这类DC/DC输出纹波20mV以内都是可以的。而且还要注意测试,很可能是测试误差。

       如果你需要确认这个差异,首先要确认测试,然后严格参考datasheet layout, 这些有可能影响输出纹波。