使用bq24610芯片遇到问题,现在给电池充电大约有4.5A充电电流,但是现在结束充电电流设置0.3A,实际使用万用表测量,电流到达125mA 才会跳灯,STAT2灯亮,不知道为什么现在一直在纠结这个问题。麻烦TI技术支持解决一下,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,请确认Rsense阻值多大,如果使用的10mohm的电阻,和数据手册的默认值是一样的125 mA
建议您用 bq246xx Calculation Tool V1.5确认电路元件的参数。