This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: REG1,REG2

Part Number: BQ76952

1 电流

1.1 CC1每250ms上报一次,若没有标志位,还有其他方法能保证MCU能及时读取到最新的CC1吗?

1.2 CC3作为80(缺省值)个CC2的平均值,是每3ms(缺省值)更新一次,还是每240ms更新一次?可以通过ADSCAN标志位来判断CC3是否更新了吗?

 

​2 REG1和REG2

由于REG1REG2上电时默认是没有输出的,我们想要其上电是有输出,需要进行OTP操作,但在此之前需要REG1REG2有输出,保证对MCU的供电,

在参考手册中提到了使用 “外部电压电源过度驱动REG1电压”,请问这个过度驱动该如何操作?