This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25756: STATE1和STATE2的状态一直01、10的切换,不稳定。

Part Number: BQ25756


调试BQ25756芯片时,STATE1和STATE2的状态一直01、10的切换,请问可能是什么原因导致?

基本设置如下:

1. 输入25~30V,输出端接上电池组(电池组电压25.6V);

2. CE已拉至低电平;

3. 开关频率300KHz,电阻100K;

4. 输入电流限制6A,电阻3.3K,采样电阻5mR;

5. 充电电流限制5A,电阻10K,采样电阻5mR。