This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1: Register Setting

Part Number: BQ40Z50-R1


Mr/Mr:

What information about the manufacturer is recorded in these four register?

What the default values(0x61,0x62,0x63,0x64) mean?

I want to turn off the internal resistance check function,what should I do?

  • 您好,There isn't much to these registers, you don't need to configure it in any way for the gauge to work. These blocks provide some extra storage that the customer can use however they like. The TRM contains information on how to read/write these blocks your customer can reference.

    Section 13.1 in the TRM has a guide and some examples to read and write to the manufacturer access blocks, which includes these two blocks.

    internal resistance check无法关闭。如果做充放电就会读取RA table的参数来计算容量。