BQ76952 第46PIN (CP1)上的电容,最大容值为2.2uF;当使用2.2uF±20%电容,按精度计算最大容值已达到2.64uF已超出范围;此情况是否可以使用??或者会造成什么影响??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
BQ76952 第46PIN (CP1)上的电容,最大容值为2.2uF;当使用2.2uF±20%电容,按精度计算最大容值已达到2.64uF已超出范围;此情况是否可以使用??或者会造成什么影响??
您好,请参考下面内容
The CP1 is the charge pump of the BQ76952. The charge pump provides a voltage higher than the battery voltage (typically 11V) to Turn-ON the CHG/DSG FETs. So, CP1 is basically the supply for the CHG and DSG drivers.
Using a CP1 value capacitor greater than 2.2 uF increases the rise time of the Charge Pump, and FETs might turn ON while charge pump is still transitioning from low to high. Using a CP1 capacitor larger than 2.2 μF is not recommended with the BQ769x2 family devices.
For more details on the Charge Pump pin, please see section 4 Charge Pump (and FET Turn On)