This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM317A: LM317A Thermal Dissipation

Part Number: LM317A
Other Parts Discussed in Thread: LM317

LM317A SOT-223 package TJA is 59.6,  Tj= Ta+ (Rja*Power). Power=(Vin-Vout)I
So, if I use LM317A in TA= 85C, I=1.5A design, Vin-Vout shoud less than (TJ-TA)/Rja=(125C-85C)/59.6=0.67V? am I right

Is there any solution to improve heat dissipation without  adding additional heat sinks. in order to get I=1.5A , Vin-Vout> 4V using conditions

thanks!

  • HI

        一般如果功耗导致芯片发热较大,建议用DC/DC, 效率非常高,一般不必担心芯片散热。如果担心layout空间,可以选择模块电源。如果一定要选择LM317,  选择热阻较小的设计方式,例如Junction-to-case (bottom) thermal resistance。

  • Hi Johnsin

        设计应用是动态可调输出,所以317会比较合适

        如果是JC(Bottom)的方式,是不是就理解为以PCB thermal PAD作为散热介质,设计PCB的JA=(TJ-TA)/Pd。这个Pd是(Vin-Vout)*Id还是(Vin-Vout)*Id-(TJ-TA)*317的JA。换句话就是计算PCB面积的时候计算公式中用到的发热功率,是不是要刨除317通过case上表面散出的热量

        多谢

        

  • HI

       动态可调只是需要可调的反馈信号给到芯片即可实现,一般选择LDO并不是适合,除非功耗很低。

       JC(Bottom)参考: www.ti.com/.../spra953c.pdf