This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
4串最低容量为14.5Ah的电池包学习成功后按照0.5C进行充放电循环;
多次循环后查看Log数据,发现有以下问题:
1、Cell Terminate Voltage设置为3000mV,但是RSOC、RM总是在12.4V左右为0,而不是在12.0V;
2、使能RMFCC功能,但在充满静置2h过程中RM逐渐减小,该怎样调整配置使其在放电时才开始降低?
3、最后2个循环的FCC突然偏小,由14190mAh跳变至8919mAh;
附件为bq34z100-g1的gg文件、Log数据以及化学ID,麻烦分析下原因,谢谢!B0859-ID2349-study-2023-12-18.gg.csvB0859-ID2349-0.5C-2023-12-14 .csvroomtemp_rel_dis_rel-report-2023-11-2.zip
您好!非常感谢您提供相关资料;
电池包的设计容量是14.5Ah=14500mAh,没有超过最大值;
设计能量是=14.5AH*3.65*4V=211.7Wh=211700mWh,超过了Design Energy的最大值32767mWh;
将Design Energy设置为21170mWh,Design Energy Scale设置为10;
电流按照实际电流校准(例如1A放电,校准电流也为1A),那么需要开启Pack Configuration:SCALED功能吗?
之前在最后几个循环测试时恰好遇到寒潮,天气突然降温,所以当时电池包周围的环境温度会突然下降;目前怀疑FCC突然降低与温度有关,需做相关测试验证这点;
另,这个项目所使用的电芯需要定制化学ID,麻烦提供下相关资料与电芯的收件地址。
您好,在E2E英文论坛发帖已经回复,请关注该帖。
e2e.ti.com/.../bq34z100-g1-gpcrb-firmware-is-not-explicitly-supporting-ra0_ch