Part Number: BQ24610
Hi
我司采用BQ24610,输入12V,输出8.4V。最大充电电流5A,截止电流200mA。该方案已经使用批量10K左右,但近期新生产出现4PCS充电,在1A左右停止充电,电池未满。
交叉验证问题跟随PCBA走,想咨询下,应该怎么排查该问题,哪些电路可能会改变截止充电电流。
已排查:
1. Iset2电压0.187V和正常一致
2. 截止后电池更换到其他单板,可以继续充电到预设200mA截止

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.