This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25730EVM: 2S电池,当快充满时,充电异常,突然掉到0.

Part Number: BQ25730EVM


1、使用充电板进行电池充电,电池是2S,满充电压是8.8V,最大充电电流5A。

2、使用Battery Management Studio V 1.3.124进行充电测试,设置项:Charge Current :5A . Max Charge Voltage: 8800mV。当电池从无电开始进行快充,充电可以达到设定的5A值,当电池电压到8.6V左右时,充电突然断掉,显示0A.

此时寄存器值:Charger Status 还是显示快充状态。

带着充电头,Vsys和Vbat都是8.8V,拔掉充电器后,Vbat和Vsys只有8.55V左右。

3、按照正常逻辑,电池电压到8.8V 之前,应该都会以大电流充电,当到达8.8V,才进入恒压模式。

请问问题2如何进行排查,谢谢。