在1.012V到5.566V的过压保护精度是±3mV,但是相同环境温度下,3.036V到5.06V的过压保护精度最小-15mV,最大15mV,实际应用中过压保护的精度究竟以哪个为准?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在1.012V到5.566V的过压保护精度是±3mV,但是相同环境温度下,3.036V到5.06V的过压保护精度最小-15mV,最大15mV,实际应用中过压保护的精度究竟以哪个为准?
您好,The ±3mV is the typical accuracy. This would be the close to the typical, if not better, for the 3.036V to 5.06V range. Which is not displayed, but would be essentially warrantied since the range is smaller than the 1.012-V to 5.566-V range.