This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.我的LM5026方案。24-130V输入,12.5V/15A输出。VCC连接VIN,外部12V供电。
2.输出反馈,典型的基于LM2904做的恒压恒流方案。
3.调试发现,系统很不稳定。
轻载,出现PWM异常。
40V输入,1A负载,会异常PWM
50V输入,大概1~3A,异常PWM
60V输入,大概1~7A,异常PWM
80V输入,大概1~10A,异常PWM
(通道2:OUTB、通道3:Vds)
带重载,即除上述负载外(15A以内的),PWM正常
4.调试中,轻载打出PWM,占空比有13%。只要带轻载(大概1A),占空比随即翻转至对应的占空比(依据理论设计)。
5.带载启动,PWM无法连续打出
空载无问题,空载启动再带载,PWM连续
目前有调整环路等,但都无改善。
是否有上述问题,能给予一些思路?
HI
将电路传上来看看?变压器设计是借助Power Stage Designer 5吗?