我运用TPS75003,做电源管理,完全按照他的典型电路来做的,最后输出3.3V,2.5V,1.3电压,理论值是3.3V,2.5V,1.2V.但是我一接入FPGA2.5V的电压不变,3.3V变为1.3V,1.3V变为0.2V,都换了好多电源芯片和FPGA的芯片,但是结果还是一样。伤心欲绝
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我运用TPS75003,做电源管理,完全按照他的典型电路来做的,最后输出3.3V,2.5V,1.3电压,理论值是3.3V,2.5V,1.2V.但是我一接入FPGA2.5V的电压不变,3.3V变为1.3V,1.3V变为0.2V,都换了好多电源芯片和FPGA的芯片,但是结果还是一样。伤心欲绝
我在想是不是我的电路中的100uf的电容不够大才出现我说的那种情况啊,但是典型电路是这么干的,应该不会出现什么问题啊。
非常感谢您,经过你这么一说我刚才又看了看它的芯片手册,我发现我选的器件跟它典型电路里面的还是有点不同的,除了您说的电阻外,我发现我我的肖特基二极管啊,电感啊,虽然值是一样的,但是封装还不一样,比如它有个肖特基二极管是ss32封装,我选的是ss14。不过这个或许问题不大,但是最重要的或许是您说的我用的电阻太大了,没有电流通过,导致电路不正常。因为我都不知道有毫欧这种电阻,我是电路小盲人,真的非常谢谢您。谢谢您的帮助。
您好,我今天买回来了毫欧电阻,确实像你所说的那样,电源能带负载了,3.3V的输出为3.35,,2.5输出为2.56,但是1.2输出端却为1.44,这个电压相差有点大,换了电容电感都不好使,都是这个值,请问我该则么办