This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62585: 應用線路確認

Part Number: TLV62585

Hi all,

我司RD 使用TLV62585PDRLR於外接式SSD產品

電路與Layout請參考如下,

使用條件: VBUS5VVDD 0.9V,其中電路中的 C42, BC52目前未上件,L11uH,目前負載部分約0.8A to 1.2A

 

L8

L6

Output to SW Length about 400mil

 

有以下問題希望可以協助確認

  1. 是否可以使用電容BC52 以加強輸出電源的穩定性如可,是否會有副作用?
  2. 承上題,請問其建議的Value為何(根據Datasheet 5V8V 22pF)? 目前使用18pF是否適用?
  3. 請問Layout 設計是否有建議調整的地方

謝謝