This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5116: 关于LM5116技术问题

Part Number: LM5116


你好,

     在使用LM5116进行电路设计 时,遇到如下问题(电路图如下),请帮忙解答一下,谢谢!

1、L25的封装或者DCR选择多少,会让U27及电感的发热量会最小(满载12V 5A温升多少,空载发热量也要最小),以下电路L25的耐温多少,请提供详细计算结果。

2、用以下电路的情况下,U27在空载的情况下自身发热严重,这个是什么原因引起的,如何避免这个发热的问题?

3、这个电路需要输出3种电压(4.3V 5A,8V 5A ,12V 5A),Q6,Q7的选型推荐,需要提供详细计算结果(Rds(on)热阻温升)。

4、输出上述这3种电压,能否用DAC灌入FB脚实现,有没有推荐电路,这样做有没有风险?

5、R165用四端子电阻和普通电阻采样,差别会有多少?

6、满载输出时12V5A,8V5A,4.3V5A时,输出电压纹波是否能在正负20mv以内,输出电压是否能在正负50mv,电容,电感如何选择?

  • Hi

        电感DCR尽量小即可,这个可以减小电感的功耗,但是不会影响到芯片。对于芯片功耗,需要尽量选择Qg,Rdson尽量小的MOS, 前者可以减小芯片功耗,后者可以降低MOS功耗。另外就是降低功率频率(推荐300kHz左右)。

        按照你的设计,补偿电路建议按照8.15V设计,如果纹波达不到要求可以在输出增加一级LC.  (对于外部补偿电路的芯片,一般不建议做输出可调,除非调节范围很小)。

        输出可调,DAC 通过二极管,电阻给到FB即可实现。纹波在50mV应该没有问题,如果需要更小,如上建议增加LC.