This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: SPI 读写速度

Part Number: BQ76952


Hi

我们在测试BQ7695204时发现SPI读写的速度太慢,远超我们的预期,严重影响到其他代码的运行。

经过测试发现在读取时,在第二次读取时才能将想要的数据及CRC值读取出来,这就导致BQ7695204读写寄存器所花费的时间远超我们预期值,

请问在保证CRC功能的前提下,有没有办法解决SPI读写寄存器过慢的问题?

 

当前SPI 时钟频率为0.26MHz,我们最高能提高到0.31MHz,但这容易导致SPI CRC校验失败从而重试

下表是我们测试读取不同数量寄存器所花费的时间

 

寄存器读取时间

 register name

 address

 time(ms)

 cell1 voltage

 0x14-0x15

 1.66

 cell1-cell15 voltage

 0x14-0x31

 36.3

 DASTATUS5

 0x0075

 39.7

以下是这几种情况的实际波形

1 读取cell1 voltage0x14~0x15)的波形

从波形很明显能看出,在读取cell1 voltage时,读取了两次0x14寄存器和两次0x15寄存器,这就导致SPI 读写时间近乎翻倍

2 读取cell1~cell15 voltage的波形

和前一个波形一样,每个寄存器都读取了两遍