This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5122: 为什么对Power Supply的电源要求是25A,这个值是怎么得出来的?

Part Number: LM5122


这是LM5122EVM-1PH Evaluation Module User's Guide上的截图

可以看到上面对Power Supply 的要求是25A,用户指导中的原理图的输出的最大电流是4.5安,输入的最大电流是15安。都远小于25A,为什么这里要25A?是因为原理图上电感的的IDC快接近25A了吗?

  • Hi

       这个是应该而非必须,要看你选择电源供应器的规格,一般是20A甚至更高。 而实际上18A以上就应该没有问题。

      (按照最高24.84*4.5=111.78W输出,最小9V输入,效率95%, 平均输入电流111.78/95%/9=13A,   那么最大峰值输入电流为13*1.2=15.7A,还必须预留一些余量,因为要高铝输出可能要高于4.5A的情况)