利用LM3409HV芯片恒流给镍氢电池充电,输入电压在40~65V之间,输出电压24~35V,根据PDF文档画出了电路,但是实际使用时不接负载有输出,电压为输入电压,但是接了负载之后电压直接变为零。请问是什么问题呢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这个功率比较大了,
1.是否有器件比较热,比如MOS管,电感。
2.建议在电阻R3的上端和 二极管D1的下端之间接上一个低ESR,ESL的电容。
Hi
输入建议100uF + 10uF陶瓷电容,靠近电感。
注意一下你的电感选择, 将电感适当的选大一点,例如47uH~100uH,(具体看你的参数计算的基础上加大一点)
饱和电流要足够,大于你最大充电电流的1.3倍数以上。
Hi
另外注意一下layout, 零件尽量靠近一点,避免寄生参数的产生。