Other Parts Discussed in Thread: LM5122, BQ24630
当挂负载正在工作中,手动关闭AC-DC的24V开关电源时。LM5122会偶发出现同步升压达不到设计值24V(其值为19.303V),在保持上述状态(负载电机转动工作)时,这种异常延时2.56s时长。才可以恢复正常的升压值。
电池采用的充电IC型号为:BQ24630,VBAT=20.94V,附上上述测试波形,OK的测试波形和NG的测试波形及其部分电路图。说明一下,此异常会触发其他的电路报欠压预警。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
电路打不开,可以直接通过下面的“插入”贴上看看.
请问,如果用电源供应器供电是否可以正常? 另外LM5122功率电感饱和电流建议再适当放大,输出电容也建议放大一些,原因是你带的是感性负载。