This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61089: TPS61089芯片运行一点时间后输出电压跌落,ILIM(8引脚)电压变到3.8V左右

Part Number: TPS61089

使用TPS61089芯片做升压电路,输入电压3.3V~4.2V,输出电压9.4V,400mA。

在使用过程中,发现运行一段时间后,输出电压跌落到6V左右(后端设备开启电压为6V),然后测试ILIM引脚电压变成3.8V左右了(RILIM电阻为150K),有时还会出现是好是坏的情况。有时运行短时间就会出现,有时需要运行好几天才会出现。目前已经有10块左右的电路板都出现这个问题了。在这种情况下,如果把负载去掉,电压可以回到9V~10V,会出现波动,不稳定。

请问在什么情况下,ILIM引脚引脚电压会由1.21V变到3.8V?

期待您的指导。