我们有个产品使用了两颗TPS61196,两颗芯片是同样的电路,设置电流为140mA,正常工作时为60%占空比,测试发现两个芯片输出的RMS电流分别是85mA和80mA,是否属于正常误差?
若不属于正常误差,还请告知正常误差应该为多少?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
精度差异超过5%是有些大的,Iset的电阻精度是否选择1%, 输出电压(LED电压)上的纹波是否异常?
Hi
应该是严重偏大(不好意思,笔误)。
一般测试带宽20MHz即可,纹波一般几十个mV(<50mV)。
将输出电容再放大一些,到100uF., 另外严格参考datasheet的layout。