Part Number: TPS6594-Q1
Other Parts Discussed in Thread: MSP432E401Y
问题1:
通过 MSP432E401Y MCU Launchpad 的调试板卡,通过GUI连接TPS6594芯片,出线连接不稳定,时好时坏,I2C上拉电阻1.5K. ,可以连接MSP432的板卡,但连接不上芯片,采用的GUI版本为最新的4.0.

问题2:在GUI中,加载J721E的配置模板,在做PSFM验证时候,发现了2个error,分别是act2socpwrerr和any2act两个故障

问题3:但偶尔连接TPS6594芯片成功后,快速启动按钮自动识别器件操作中,只能识别一个芯片。芯片的地址为0X4C。

问题4:连接一个芯片成功以后,烧写J721e的模板配置,不能进行烧录,报出不能解锁EPROOM的故障,万用表测试芯片的实际输出,芯片也没有实际的电压出来,所以NVM未烧录成功。

以上问题请TI专家尽快帮忙解决。谢谢!