This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5122: 实际输出电压(22V)比目标输出电压(24V)小2V左右。另外,实际输出电压不能维持在22V,会逐渐降低。

Part Number: LM5122


我按照lm5122 规格书中的电路做了一个typical input voltage :12V,output voltage:24V@4.5A的板子。

实际测得输出电压为22伏左右,并且,电压刚达到22V就会往下掉。