我按照lm5122 规格书中的电路做了一个typical input voltage :12V,output voltage:24V@4.5A的板子。
实际测得输出电压为22伏左右,并且,电压刚达到22V就会往下掉。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我按照lm5122 规格书中的电路做了一个typical input voltage :12V,output voltage:24V@4.5A的板子。
实际测得输出电压为22伏左右,并且,电压刚达到22V就会往下掉。
Hi
带载4.5A测试出现上述异常吗? 如果轻载启动呢?
首先确认功率电感饱和电流足够大,并且输入电容足够大并layout上靠近功率电感(以及sense电阻)。
其次确认过流保护信号是否有noise导致提前保护。
不是带载4.5A出现上述异常。是把负载调成定电流模式,并且限制最大电流为0.1A,出现上述情况
饱和电感达到了32A够吗?输入电容和datasheet上的一样可以吗?还是要比它更大?
过流保护信号会让芯片进入hiccup模式对吗?
Hi
饱和电流够的。
采用电压模式是否正常?