Other Parts Discussed in Thread: LM74502,
您好
使用LM74502芯片时,有如下问题,期待您的解答。
1.按照LM74502EVM中设置36V过压钳位,在200V抛负载试验中,输出端电压是否能够小于40V。
2.LM74502或者LM74502EVM是否进行过ISO7637-2、16750-2相关测试,能否提供试验中的输出电压波形。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好
使用LM74502芯片时,有如下问题,期待您的解答。
1.按照LM74502EVM中设置36V过压钳位,在200V抛负载试验中,输出端电压是否能够小于40V。
2.LM74502或者LM74502EVM是否进行过ISO7637-2、16750-2相关测试,能否提供试验中的输出电压波形。
HI
1. 能否具体说明下200V抛负载试验 ? 我们没有针对这样测试的文档说明(我这边也没有板子来验证这个测试)
2. LM74502或者LM74502EVM没有提供ISO7637-2、16750-2的相关测试信息。