This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL431: 使用TL431构建环路补偿网络时,低频相位偏移的问题

Part Number: TL431


如下图所示,使用TL431+PC817搭建了III型补偿网络,并仿真了补偿网络的波特图,其中TL431使用了TI官网下载的SPICE模型,PC817使用了理想的电流控制电流源来替代

III型网络是反相放大,同时伴有一个初始极点,因此初始相位应当是-270°或者超前90°,然而经过仿真看到的Phase波形在低频处产生了偏移,这与使用常规OPA或OTA搭建的补偿网络是不同的,请问这是什么原理?

如下图所示,是简单的基于OPA的III型补偿网络的波特图仿真,在低频处的相位基本没有太大的偏移,复合预期

以上低频相位偏移现象在I型,II型号补偿网络中都有出现,当频率增加到10Hz左右时,TL431补偿网路网络的相位就会达到预期的+90°/-270°,请问这样现象的原理是什么?是由于TL431本身的频率特性导致的吗?

  • Hi

         我建议你将这个问题放到美国E2E上一下: https://e2e.ti.com/

         TI有一些文档上提供上述波特图,但是对于设计原理以及调试方法之类没有详细的描述,建议你找一些电源书籍如开关电源设计原理之类,里面有大篇幅的描述。或者你在美国E2E上问一下,他们应该有一些额外的文档有描述这一块。