This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ4050: 低温放电

Part Number: BQ4050


Hi

我们在使用贵司BQ4050做便携式储能项目时,低温放电SOC会大幅度跳变,并且用 CEDV 算法电量计计算出来的CEDV 参数不太适用。因为依据报告显示使用CEDV参数后常温和高温下SOC精度会受比较大的影响,所以为了常温和高温情况下的SOC不受影响我司目前的SOC算法没有开启CEDV功能。然而,这样导致低温的时候SOC跳变的很厉害,所以请问贵司针对BQ4050方案的低温放电SOC大幅度跳变的问题还有什么解决方法和意见吗?期待你们能抽时间帮我们分析解决这个一直困扰我们的问题!(跑CEDV 参数所做的数据、BQ4050的配置以及我们的产品低温放电的数据请见附件)。

CN061-GW1.3-20231107.gg.csvCN061-整机低温环境下-8℃ AC+PD满载放电 SOC从99%跳至1%.csvCN061-跑电量计(3).rar