This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于固定输出2.5V电源芯片选型问题



您好,我现在需要一款固定输出的电源转换芯片,要求固定2.5V输出,输出电流不小于0.5A,输入电压12V,封装要求TO-252或TO-263.麻烦推荐几款符合条件的芯片,并给出参考设计。

  • 亲,因压差太大,对于最大0.5A电流负载,导致线性方案的实际损耗会达到5W级别,因此,最好用开关方案。

    从亲的字里行间,可以看出想要简单易用的方案,基于此;建议千万要弄清实际负载情况。过大预度对这个应用并不合适。如此应用,如果能降到200mA,那就可以用LM3337-2.5的LDO,电路会简单许多。

    好了,对于这个级别PWM稳压,只需要SOT-23-5封装IC就可以了,建议看看TPS5602000。