·负载电流为8A时,显示电流为8A 表现是准确的。
负载电流为20A时,显示电流约为20A 表现是准确的。
负载电流为25A时,显示电流为24.346A 表现是开始出现较大的偏差。
负载电流为30A时,显示电流为24.398A 表现是电流已经停留在这24.3A数值这里的。
请问我这哪里的设置出现了问题?怎么样去解决?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.