This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ4050: BQ4050 电流超过负载25A后显示值与实际电流偏差大

Part Number: BQ4050


·  负载电流为8A时,显示电流为8A 表现是准确的。

   负载电流为20A时,显示电流约为20A 表现是准确的。

  负载电流为25A时,显示电流为24.346A 表现是开始出现较大的偏差。

  负载电流为30A时,显示电流为24.398A 表现是电流已经停留在这24.3A数值这里的。

请问我这哪里的设置出现了问题?怎么样去解决?