使用BQ25723给4串电池进行充电,不插电池时,接入DC电源(24V),REGN输出电压为6V,单独只接电池时(电池电压15V),REGN输出电压为9V左右,DC电源和电池同时在时REGN电压也为9V左右,想知道为什么会出现这样的现象?合理吗?看手册上REGN电压应该是在6V左右。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用BQ25723给4串电池进行充电,不插电池时,接入DC电源(24V),REGN输出电压为6V,单独只接电池时(电池电压15V),REGN输出电压为9V左右,DC电源和电池同时在时REGN电压也为9V左右,想知道为什么会出现这样的现象?合理吗?看手册上REGN电压应该是在6V左右。
您好,请参考下面的schematic checklist 确认电路和layout
0552.BQ2570X_BQ2571X_BQ2572X_BQ2573X_SchematicChecklist.pdf
For layout guidance, please see the following FAQ.
https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1032723/faq-how-do-i-ensure-the-charger-layout-is-satisfactory-is-there-a-guideline-for-the-buck-boost-charger-controllers-like-bq25713-bq25720-and-bq25730-etc
您好,There should not be 9V on REGN. I notice that the COMP1 and COMP2 compensation networks are not following the guidelines as specified on the datasheet section 9.3.13. Also, the ILIM_HIZ should be powered from a voltage divider network from VAA, not from REGN. If the REGN still does not show 6V after changing the compensation network, you may need to change the IC.