使用TPS652661做稳压电源,输出3.3V/3A,1.2V/2A,1V/2A,空载时可以,带载时,1V输出将为970mv,1.2V有周期性毛刺,3.3V电压会产生振荡,请问有没有大佬指教一下啊。
下图是我的电路图和3.3V的震荡图。
电路图中PVIN1设计错了,已飞线接到5V。调整过程中将L6修改为3.3UH也没用。是不是被必须得4.7uh,或者COMP补偿电路哪里有问题?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
首先建议你确认一下功率电感饱和电流足够大,其次注意GND布局以及功率回路尽量小, 这些都容易导致芯片带载能力下降。
Hi
空载异常带载正常一般是建议确认补偿电路的,这个一般不是PSM模式导致的. PSM模式相对CCM模式纹波会大一些,但是一般也不会超过50mV.
另外建议你严格参考datasheet layout.