This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5166: 电源设计咨询

Part Number: LM5166


工程师您好,我想用LM5166Y设计一个输入电压12V,输出电压3.3V,最大输出电流300mA的电源,这是网站上设计工具给出的设计方案:

我想把47uF的输出电容Cout用5个10uF的电容并联替代,不知道这样可不可行?下图是我的原理图: