期望设计:电压输入15-48V;电压输出:60V;电流输出:1A(MAX)。
我将WEBENCH建议的Ruvb从5.11k改为4.3k后,电感不发出蜂鸣声,电压输出可达到60V。同时,
电子负载在定电阻60欧姆,定电流1A,定功率60W的情况下,板子都能输出:电压60V,电流1A。
可是在定电压60V模式下,板子只能输出60V电压,输出电流为0A。这是什么原因造成的呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
期望设计:电压输入15-48V;电压输出:60V;电流输出:1A(MAX)。
我将WEBENCH建议的Ruvb从5.11k改为4.3k后,电感不发出蜂鸣声,电压输出可达到60V。同时,
电子负载在定电阻60欧姆,定电流1A,定功率60W的情况下,板子都能输出:电压60V,电流1A。
可是在定电压60V模式下,板子只能输出60V电压,输出电流为0A。这是什么原因造成的呢?
1.我上图给你看一下。


过了15秒左右,电流升到了1.2A



定功率模式下,先是输出电压:15V,输出电流:3.7A,然后才是输出电压:60V,输出电流:1A

2.是的,用的是电子负载。