您好!
如《BQ24600手册》7.3.3预充章节所述,预充可能导致状态引脚故障。最小预充电电流限制在125 mA左右,默认为10-mΩ感应电阻。我用的10-mΩ电阻器,充电电流是预充电流的10倍,充电电流应该大于1250 mA吗?现在我将充电电流设置为900mA,状态引脚显示故障。设置充电电流为900mA会导致状态引脚故障吗?
Best wishes!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,可以设置9A充电,预充电流是0.9A,提示错误可能是30分钟没有充到Vlow threshold。请参考bq246xx Calculation Tool V1.5 确认电路参数。
您好,已经在E2E英文论坛发帖,需要查看您的波形然后向您提供反馈。