This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求教,做一个输入<3-14V的宽输入,输出+5V电源,电流1-2A用于低噪声放大供电

Other Parts Discussed in Thread: LM2941, LM2611

是否有现成的单个DC-DC芯片满足设计指标要求?噪声纹波要足够小,串入射频链路无影响。如果没有采用DC-DC+LDO的形式,采用LM2611芯片输出-5V后再加一级LM2941转换成+5V可不可行?这样设计是否过于复杂,工作环境用于-40~+70度是否能满足。请有经验的朋友帮忙。本人专门做射频的,对电源不太了解,整个模块电流大概500mA,要留多少的电流余量。

  • 一般;适当的LC构成的派型滤波器就可以抑制电源对射频电路的影响。LDO通常无能为力。因此;DCDC+滤波器就够了。一般对于电源,需要按数据表;依电源输出与温度关系查表获得答案。对于比较稳定负载,通常可以取额定容量的30%~70%,作为负载可用量。

  • XP 说:

    一般;适当的LC构成的派型滤波器就可以抑制电源对射频电路的影响。LDO通常无能为力。因此;DCDC+滤波器就够了。一般对于电源,需要按数据表;依电源输出与温度关系查表获得答案。对于比较稳定负载,通常可以取额定容量的30%~70%,作为负载可用量。

    请问有没有合适的芯片推荐呀,我在里面找了些,但是不是大了就是小了。人都搞死。

  • 亲,你的电源输入范围多少?

  • XP 说:

    亲,你的电源输入范围多少?

    我就是保证输入5V和12V左右两个电压模块能正常工作,一般是这两个电压输入,当然可能有时候有点压降