This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1: BQ40Z50-R1设计中FUSE异常状态

Part Number: BQ40Z50-R1


1、第一次中,FUSE功能没有应用,处于悬空状态,如下图:但在测试状态中,时常FUSE标志位会置起,导致不能使用;

2、第二次中,经过改善后面将FUSE引脚直接接入到GND,如下图:测试中未体现出异常,但是在客户端使用的时候,整体电压约14.7V左右,通讯正常,但是断开上位机与板通讯后20秒,输出无电压,接上位机通讯后,依然为FUSE置起,复位后FUSE标志位清除,输出正常;重复断开上位机与板通讯后20秒后,依然无输出;

3、第三次中,将FUSE引脚经过下拉电阻270K到地后,验证无以上两种显现出现;

疑问点:
BQ40Z50-R1技术手册中,FUSE引脚定义功能说明中,FUSE不使用时候需要接地,为什么直接接地后也会出现这种状态,经过下拉到地中串联一个200K多的电阻到地后就可以解决这种问题,这中现象应该如何理解呢?