This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5122: 电子负载定电压模式下只输出电压,不输出电流

Part Number: LM5122


期望设计:电压输入15-48V;电压输出:60V;电流输出:1A(MAX)。

电子负载在定电阻60欧姆,定电流1A,定功率60W的情况下,板子都能输出:电压60V,电流1A。

可是在定电压60V模式下,板子只能输出60V电压,输出电流为0A。这是什么原因造成的呢?