Part Number: LM5122
期望设计:电压输入15-48V;电压输出:60V;电流输出:1A(MAX)。
电子负载在定电阻60欧姆,定电流1A,定功率60W的情况下,板子都能输出:电压60V,电流1A。
可是在定电压60V模式下,板子只能输出60V电压,输出电流为0A。这是什么原因造成的呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM5122
期望设计:电压输入15-48V;电压输出:60V;电流输出:1A(MAX)。
电子负载在定电阻60欧姆,定电流1A,定功率60W的情况下,板子都能输出:电压60V,电流1A。
可是在定电压60V模式下,板子只能输出60V电压,输出电流为0A。这是什么原因造成的呢?
HI
我觉得应该是测试上的问题,我这边一般用的电子负载时chroma, 一般设置为CV模式即恒压模式是没有问题的。
按照你上面说法,负载60ohm,我这边电子负载一般是直接设置成电流。
你说的是对的,是测试上的问题。现在问题已经解决了。是电压值没设置好的缘故