Other Parts Discussed in Thread: GPCCEDV
专家你好,我想请教一下,我目前使用18650电芯,电容量为2000mAh,标称电压3.7V,满电4.2V,现在使用的过程中,电压下降到3.6 RelativeStateOfCharge 显示电量百分比为零,但是我的目标是想让他下降到3.0V再让RelativeStateOfCharge显示为零。我查了手册,但是没有找到相关的设置,但是我在论坛上看到别的电量芯片有Terminate Voltage这个参数,但是BQ34210-Q1的手册并没有这个参数,
是否BQ34210-Q1的默认 Terminate Voltage 就是3.6V?
我是否需要再设置 Reserve Capacity ,才能让电芯工作到3.0V?
能否让电芯工作到3.0V后 RelativeStateOfCharge 读取值才下降到零?