This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: BQ76952的充电和放电驱动能力

Part Number: BQ76952

    您好!

    客户在开发BQ76952 时有个问题要请教您,当电池额定电压是12V4串电芯)和24V8串),充放电驱动电平只有10.35V,实测自举电容上的电压10.6V。自举电容选择470nF,二极管D19选择肖特基二极管,实测压降0.17V。而当电池额定电压在48V(15串电芯)时,自举电容上的电压是11.1V,充放电驱动电平可以达到10.8V。所以产生了3个疑问:

      (1)芯片的标称充放电驱动电流有多少,驱动电平有多高?

      (2)为什么48V平台的自举电压比较高11.1V,而12V48V的驱动电压比较低10.6V,这是芯片自身的特性还是说和驱动电路参数设计有关系;

      (3) 在12V24V平台,试着将自举电容调整到1uF1.5uF,自举电容上的电平还是10.6V不变,要如何调整参数或调整电路才能使驱动电压抬高?

       

        以上问题,期待您的解答,下图是充放电驱动和主电路参数的设计,也一起帮忙看下是否合理,谢谢!